I am planning to use the TPS56121 DC/DC Converter in a new design and have acquired the TPS56121EVM-601 evaluation module.
Unfortunately when monitoring the 1.2V output we noticed a 150mVpp ringing at approximately 200MHz every time the converter swtiched. This dampens down after about 10 cycles.
This noise is also more dramatically evident on the 12V input side though at over 1.5V in magnitude!
The Eval modules user guide has a graph that claims the output ripple noise should be around 20mVpp. However, on closer inspection, it does note that the bandwidth of the probe is at 20MHz! So what we are seeing could be correct???
Can TI support confirm or deny this feature that we have observed on the TPS56121EVM?
This will be un-usable for my application in the current state as I need a stable supply with less than +/-5% noise at 1.35V with switching load current changes of up to 10 Amps.
thanks
Allan