Tool/software:
Dear Sir,
We have designed a BMS with 6s configuration with each cell can charge maximum up to 4.2 V resulting overall BAT voltage to 25.2 V. Now as these BMS is assembled in a battery pack I have certain doubt related to waking up the BMS in a pack. As, we are now designing a battery charger board to charge our battery pack, now suppose if my BMS goes in shutdown mode. I am providing 28v power to my battery charger board through a battery adapter for waking BMS. Now I am generating waking voltage for pack 25.2V by droping 28v through 4 series diode as shown in attached images and current limited to pack is 50mA through a series resistor. Now suppose, initially my battery Pack is shutdown and I have connected the V_Pack terminal to my battery Pack+ terminal. So, voltage available at V_PACK terminal is 28V till my battery pack won't wake up. As soon as, my battery pack wakes up by these 28v and if it demands currents then there will be drop of 0.7V across 4 diodes resulting voltage at my V_PACK terminal as changing from 28V 25.2 volts.
1) So, sir I want to know If I provide voltage at my pack 28V initially for waking up my BMS will it be OKK? If my bms wakes up and demands current then drop occurs and V_PACK changed to 25.2v. Will these sudden change from 28V to 25.2V will do any damage to my BMS?
I have attached image of battery pack voltage generation please refer it for your reference.
Waiting for your reply,
Thanks & Regards,
Shubham