This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: max cell balance resistor

Part Number: BQ76952

Tool/software:

Hello Ti Team,

we are using the bq76952 in host controlled 13S application with internal balancing.

We are using 200 Ohm balancing resistors and 0,1 µF capacitors.

Please look at the following schematic:

In the datasheet and the faq (sluaaq5) is written that the max value should be 100 Ohm.

Could this be a problem?

Thanks for helping us.

Regards, Klaus.