Other Parts Discussed in Thread: , TPS65400
Tool/software:
Hello - I'm designing a non-standard, 2W inductive power system that will operate in the 100-1000kHz range. I would like to be able to adjust the secondary side voltage during low load to minimize power losses.
One way to do this is to shift the transmitter operating frequency further away from the pair's resonance point, like Qi/WPC.
Another way is to adjust the supply rail that's feeding the transmitter coil's H-bridge driver. For this, I'm considering an integrated-FET DC/DC with I2C control like the TPS65263.
Can you advise on potential shortfalls regarding operating frequency and control topology? I imagine that a DC/DC set to 250kHz won't be able to "keep up with" an inductive H-bridge load running at 800kHz. I'd expect subharmonics or instability might be an issue without careful sizing of output caps. I also expect there might be a preference for voltage mode vs current mode converter with a switched load like this.
Thanks!