This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC5922: Inquiry on application schematics data of LM3150

Part Number: LM3150
Other Parts Discussed in Thread: TLC5922

Tool/software:

Hi, TI expert.

I want to configure a circuit with the following specifications using LM3150.
- Vin = 24V
- Vout = 5V
- Imax = 10A

Is there any application schematics that can be provided that I can refer to when configuring a circuit with the corresponding specifications?

Please check. Thanks