Other Parts Discussed in Thread: LM5066
Tool/software:
Hi TI Team,
I would like to know more details and performance parameters of TPS2490 Hotswap controller based on our requirements mentioned below.
- Primary input from battery (15V to 30V)
- Standby input from PD sink controller (15V fixed)
- Fast Hotswap switching
- Hardware and/ or software controller
- Precise protection circuitry
Could you help us with which controller to proceed with as best fit for the mentioned requirements?
Precise switching and switching speed is an utmost requirement as this a critical part of the system. it would be great if you can guide us on this.
Thanks and regards,
Alen Abraham