This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22995: application questions

Part Number: TPS22995


Tool/software:

Hi Sir,

Could you help reply the my customer ask the below TPS22995 application questions?

Q1: Does the TPS22995 have the power-in sequence for VIN, VBIAS and ON?

Q2: The power apply to VBIAS need earlier than VIN, is it correct?

Q3: The VIN voltage cannot higher than VBIAS, is it correct?

Q4: VIN=0V, VBIAS=3.3V, ON=L; in this condition has the how much of leakage current on VBIAS?

Q5: In this design case(VIN=3.3V, VBIAS=1.2V, ON=1.8V), is it can use the 3 of different voltage on VIN, VBIAS and ON?