This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS564257: TPS564257DRLR

Part Number: TPS564257
Other Parts Discussed in Thread: TPS62914, TPS62913, TPS62903

Tool/software:

Hi,

I need help in choosing a DC DC converter considering the following requirements

Input Soruce:

  1. 5V coming through AC DC converter
  2. Five D cell connected in series 4.5 to 8.25V

I have to provide power to a 4G Module so noise and clean power is crucial.

The above power source one at a time will use but the circuit must entertain both power without changing hardware

The load current required is 3A and 3.8V.


I have been recommended that do not feed buck boost power to 4G module and add some low dropout regulator in between.

Any suggestion or help plz?

Thanks