Part Number: BQ25798
Tool/software:
1) I would like to pull up the I2C line of the bq25798 with +5V, the microcontroller operating voltage.
I am aware that this is not a problem since it is within the absolute maximum ratings, but please let me know if there are any problems.

2) The datasheet lists the specs when the I2C communication line is pulled up at 1.8 V. Do these spec values also apply when the pull-up voltage is 5 V?

3) I2C specs such as setup-time, hold-time, etc. are not listed in the data sheet.
Is it correct to understand that I2C specs not specified in the bq25798 data sheet are in accordance with the NXP standard?
(Reference) NXP Standards Documentation Page 44
https://www.nxp.com/docs/en/user-guide/UM10204.pdf
Regards,
Kagawa