This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24171: The charging current is different between the actual value and the set value

Guru 12115 points
Part Number: BQ24171

Tool/software:

Hi,

The BQ24171 is mounted on a custom board and evaluated.

The charging current is set to 884mA, but the actual value is about 1A, which is quite large.

Even if it take into account the tolerance of VREF and resistors, it is about ±1% of the set value, so I don't think the actual value should be so high.

Do you have any ideas why this might be? If you need a circuit diagram, I can share it with you in a private message.

Thanks,

Conor