Tool/software:
I used your circuit form datasheet figure 16.2. If I do short circuit on the output, BQ stops I2C (maybe goes in shutdown), DSG gate has still 1V, so DSG mosfet is partially open and the output is no more protected. I must remove Batt voltage to reset this state. If I just load more than SCD is set, everythink works fine, the SCD bit is set, after 5 sweconds is cleared.