This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3445: Excessive difference in output current

Part Number: LM3445


Tool/software:

Dear 

   At present, during the debugging of the LM3445 scheme's 25W thyristor dimming power supply (input 85-115Vac, output 28-40V 600mA), it was found that there is a significant difference in output current under different input voltage conditions;

   as following

  Input 85V and output current 550ma
 Input 100V and output current 610ma
 Input 115V and output current 700ma