This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5022: Could it do 15V->40V and -15V->-40V?

Part Number: LM5022

Tool/software:

Hi experts,

Does LM5022 could achieve +15V->+40V and -15V->-40V? If not, please kindly help to recommend suitable similar device.

BR,

Victoria 

  • Hello Victoria,

    Thanks for reaching out to us via e2e.

    I understand that you have a symmetric +-15V supply and want to connect a symmetric +-40V load.

    Is it necessary to distribute the load current across positive and negative supply?
    Or could the symmetric +-40V output be connected to +15V input only?

    Our Boost converters cannot be used to create a negative output voltage when used in a Boost topology.
    You may use a Buck converter to convert e.g. +15V to -40V.

    Or else you could use a flyback with two output windings on the transformer (driven by a single +15V input volage)
    Or, if necessary two flyback converters with a single output each, which would be the most complex constellation.

    Best regards
    Harry

  • Hi Hofner,

    Thanks for your detailed reply! Customer wants non-iso topo. 

    That's a great idea both ±40V come from +15V! What's the difference between 2 solutions: 15->40, -15->-40 ; 15->±40? I think both of 2 solution need one boost one buck. And 15V->-40V will need higher voltage buck, which will be more expensive. 

    BR,

    Victoria 

  • Hello Victoria,

    We have not talked about the power level yet.
    If it is low enough for a flyback solution and if generating both output voltages from the +15V rail is acceptable, why would the customer insist on a non-isolated solution?
    You could use one single flyback controller and a transformer with two similar output windings to create the +-40V.
    It does not need to be really/completely isolated. You can connect the GND potential from the input to the output side and you can use a simple feedback divider (no opto-coupler).
    So, you basically have one converter which gives you the second output for a minimal adder (the additional winding of the transformer, a diode and some output capacitors).

    Best regards
    Harry