This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM63635-Q1: Chips are burning out

Part Number: LM63635-Q1
Other Parts Discussed in Thread: SN6501

Tool/software:

LM63635 DC/DC converter chips are burning out.

I am doing an internship at Edorado. In my system, I used their existing design for a DC/DC converter. This design uses your LM63635 Converter IC. Previously they had issues with the ICs burning for an unclear reason. They thought to have fixed this issue by replacing the inductor in the circuit. But after 4-8 weeks of software devolpment on my system, one morning, the chip just burned up directly after turning on the power supply.

I'm told that the circuit's design is based on the reference design and/or the design recommendations, from the datasheet.

The power supply that was connected to it cannot exceed 31 V (maximum of the chip is 32V). The system is normally powered  with 24V. Powering the system directly with 3.3V, bypassing the circuit, works perfectly fine.

I will attach the schematic and PCB design as images. Another engineer is currently performing stress tests on two of the circuits, results of that can be supplied once there are results.

  • Hello

    Your schematic should be OK.

    It looks like the device is on the bottom side.

    You will need to flood the bottom with ground plane to connect all the grounds.

    It is hard to see where AGND (10) is connected; it should have a direct connection to the DAP.

    Also, try to avoid the use of thermal reliefs on the power components.

    Please ensure that the inductor is rated for the current limit of the regulator.

    Do you have another ground plane on the layer directly under the regulator ??

    Can you monitor TP1 during a power-on cycle to ensure there are no voltage spikes.

    How much load are you using during the power-on cycle ??  And what type of load ??

    Thanks

  • Hello Frank,

    Thank you for your quick response.
    -You will need to flood the bottom with ground plane to connect all the grounds
    -It is hard to see where AGND (10) is connected; it should have a direct connection to the DAP.
    -Do you have another ground plane on the layer directly under the regulator ??

    The bottom is already flooded with a ground plane (it is set to translucent in Altium to view the other layers). In addition there is an uninterrupted ground plane on layer 3 (directly below the components, layers 1 and 2 also have been flooded with ground plane.
    Pin 10 is connected to ground directly.Image: https://imgur.com/a/5IrMWBE
    -Also, try to avoid the use of thermal reliefs on the power components.
    I agree that the thermal relieves should not be around the power components, this will be updated in future versions. Although we do have another PCB with the same chip (and schematic) that also burns out at random times. In this circuit the power components have been connected directly to the ground plane without thermal relieves.

    -Can you monitor TP1 during a power-on cycle to ensure there are no voltage spikes.
    The board is powered by a bench power supply, so no voltage spikes should occur, here is a measurement that has been done without a load:Image: https://imgur.com/a/UAsilvW

    -How much load are you using during the power-on cycle ?? And what type of load ??
    There is a small capacitive load on boot up of around 46.22 uF, including the converters own output caps, after that there is an active load, the rest is resistive.
    The active load consists of 7 power isolator circuits, all using the SN6501 IC.
    This circuit uses a transformer, the transformer's data sheet states that it has a minimum inductance of 475 µH, Test conditions for this value are specified as "N1+N2/ 10 kHz/ 100 mVAC".
    Some tests have been done with an electronic load in constant current mode at 400mA. This is above the highest measured current draw of the system as a whole (with a simple multimeter). See the results:

    Image: https://imgur.com/a/JZvENxw

    Let me know which other tests can be done to further investigate.

    Kind regards,

    Gino Krol

  • Hello

    Can you monitor VCC, Vout, SW, and VIN during your power-up sequence.

    Also, can you supply a schematic of your load.

    Thanks

  • Hi Frank,

    These  are the measurements results, this is measured on a PCB with only the converter circuit on there, an electronic load was used as a load here (siglent SDL1020X-E) :
    https://imgur.com/a/9DXHfyX
    yellow is Vin, green is Vcc, orange is SW and blue is Vout.

    Within the actual circuit, there are seven units with isolated power:
    There are five isolated RS422 PulseDir Modules and two isolated RS485 Modbus Modules.
    https://imgur.com/a/B68fbRm


    Aside from those, there is a PIC32MZ2048EFH100 MCU and a UART to USB port IC:
    https://imgur.com/a/E4W5EUi

    Again, none of these schematics provided here were attached to the load during the provided test results. But they were connected when the chip burned out.

  • Hello

    You can try to re-connect one load at a time and see if it changes the start-up response, or causes damage.

    Thanks

  • Hi Frank,

    We have performed the same measurements with the full load attached, including 7 of the isolated supply circuits based on the SN6501 and a PIC32MZ micro controller:
    https://imgur.com/a/CuTmYQi

    The first two images are of the previous measurements using an electronic load.

    There seems to be some ringing in the SW signal, could that be the cause of the IC failure? If so, would it help to place bigger capacitors next to the SN6501 isolation circuits? Or would a bigger change likely be necessary?

  • Hello

    The ringing on the SW node is just the normal DCM behavior at lite loads.

    It may be a random voltage spike on the input to the regulator.  You may want to use 

    an aluminium electrolytic capacitor on the input and a transient suppressor.

    Then you can test again and see if you get any failures.

    Thanks

  • Hello

    I will close this post due to inactivity.

    If you need further help, please open a new post.

    Thanks