This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR51606-Q1: Which IOUT value should be used when calculating the inductor, the maximum IOUT operating load or the maximum IOUT supported by the converter?

Part Number: LMR51606-Q1

Tool/software:

The LMR51606-Q1 IOUT maximum is 0.6A, can I use IOUT = 0.3A to calculate the following formula?