Other Parts Discussed in Thread: TPS62170-Q1, TPS62170,
Tool/software:
Hi TI experts,
I'd like to request your analysis on an observation we have on our circuit.
See below circuit using TPS62170-Q1 as primary 3.1V regulator, and TPS73201-Q1 as secondary 2.9V LDO. this 2.9V supply is intended for the analog supply of the image sensor.
VIN regulated range = 7V to 12V
We have been observing some bad units and it looks like that the observation on the output image is related to this waveform below.
this signal is measured on C508 (input of the 2v9 LDO).
The "bands" is roughly 25Hz (currently unknown source, but there's an expected 50Hz active power mode).
The concentrated bands looks to be the active power mode and the other half maybe the low power mode.
The rms value is at 3.04V and the pk-pk is aound 80mV. The zoomed in shows that the signal has a 60khz frequency, also an unexpected frequency.
Now comparing these waveforms with a known good unit, see below diffference.
This is also captured from C508 of the known good unit.
The 25Hz band is still present, but the amplitude is significantly lower.
Zooming in, 104kHz was registered in the scope. Vrms registered is 3.04V as well.
Both units have the same circuit, and the measurement points are the same, C508 (input of TPS73201-Q1).
We are wondering, the why such difference in both units? what could have induced this unwanted higher amplitude noise/oscillation?
Additional information: C506 waveform was also measured with the unit where the higher pkpk is observed.
C506 and C508 is only separated by L503 ferrite bead.
see below C506 waveforms
Lastly, there was an experiment conducted where the C508 capacitor was removed. As per TPS73201-Q1, input, output, and Cff caps are optional. The expectation is when it was removed in the circuit, no effect on the circuit, but there was around 80khz oscillation observed. see below waveform
it would help our investigation if you could give insight as to how these observations is possible given the above circuit.
Regards,
Laud Laudencia
Electrical Hardware - Via Optronics