Tool/software:
Hi,
We use the LP2985-33DBVR in our mass prodcut, and now, we use two batchs goods in our production line( Datecode 2222+5 and 2421+5),
Now, the 2222+5 datecode is normal for the voltage drop, and the 2421+5 datecode is abnormal for no voltage output in the same design,
We are afraid if there are any modify for the chip but we can't serach the PCN file,
Please refer to below schematic diagram and advise if there are any error? and BTW, please kinldy check if there are any updete for chip after week22/2022, thanks.