Tool/software:
Dear TI Support Team,
I am currently working on a project involving the TPS61158DRVR, and I have encountered an issue with selecting an appropriate inductor. The datasheet suggests several inductor part numbers for use with the TPS61158DRVR, however most of these parts are marked as NRNDWe are specifically looking to use a 22uH inductor for our design. I came across the VLS3012CX-220M-1 inductor and would like to know if this component would be a suitable replacement for the inductors listed in the datasheet.Could you please confirm if the VLS3012CX-220M-1 inductor is compatible with the TPS61158DRVR? If not, could you recommend an alternative 22uH inductor that would be suitable for use with this IC?
Thank you for your assistance.