This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R2: bq40r50

Part Number: BQ40Z50-R2
Other Parts Discussed in Thread: BQ40Z50

Tool/software:

issue is with when battery is disconnected the bq40z50 device has no VCC and the chrg disch fets are off as not energized on their gates --put in the battery and the bq has power but is not outputting to the fet gates so it cant actually do any batt sense or charging --- - so the charger is dead unless the fets are energized  on both pack and charger sides by externally jumping ----so whats the issues ---- how do you actually wake up the bq part such that it energizes the fets and senses cell in place and allows charging to resume?

  • Hello,

    For the bq device to wake up there must be a voltage applied on the pack pin. A temporary short between the BAT and PACK pin can be implemented to achieve this. In the design of our EVMs there is a push button that can be used to short between PACK and BAT.

    Regards,

    Adrian