Other Parts Discussed in Thread: TPS1HC100-Q1, , TPS25948
Tool/software:
Please note that I got the part number confused in the title, I am inquiring about TPS1H100-Q1 and not TPS1HC100-Q1. The reason being that only TPS1H100-Q1 datasheet explains proper operation while FET is ON in reverse polarity.
I am looking for a bi-directional high side switch capable of controlling voltages between 5V to 23V and a DC current load of 2.5A or higher in both directions. Since our loads are supercaps, slew rate control is nice to have but not critical. Datasheet mentions that it does not have any protection against reverse currents and requires external components to block it.
a) Can you please suggest if this part can work for our use case?
b) Also, to minimize area on PCB, which of its external passives can be removed from the schematics?