This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS281C30: Clarification on NC Pin (Pin 8) Connection for TPS281C30

Part Number: TPS281C30

Tool/software:

Clarification on NC Pin (Pin 8) Connection for TPS281C30

 

I am currently working with the TPS281C30 and noticed a discrepancy between the datasheet and the evaluation board (EVM). In the datasheet, it is mentioned that the NC pin (Pin 8) should be left floating. However, on the evaluation board, this pin is connected to ground.

 

Could you kindly clarify which connection should be followed in practical use? Additionally, is there a specific reason for grounding Pin 8 in the EVM?