Tool/software:
Hi,
Does TPS7A57 can support 0.8V to 0.6V(0.6A) application?
I have check datasheet seems it is okay, but want double check if I miss something.
Thanks!
Jeff
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jeff,
Yes, the TPS7A57 device can be set at the specified input and out voltage application through the Rref external resistor.
Typically, we do recommend a headroom of 0.4V as specified in the datasheet:
By violating this headroom, we are unable to guarantee any of the datasheet specs as these are the minimum conditions that we test with to collect our data.
Hope this helps!
Best Regards,
Hannah