This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7B7702-Q1: impact of not using CH2

Part Number: TPS7B7702-Q1
Other Parts Discussed in Thread: TPS7B7701-Q1

Tool/software:

Hi,

  We use TPS7B7702-Q1 in our design. However, Only CH1 is used.  PIN 3& 6 &11 &13&14 are floating. Is it feasible? Will it have effect on CH1?

P.s. We know there is TPS7B7701-Q1.

 

  • Hi,

    The ENx pins have a pulldown circuit, so channel 2 will be inactive if the channel 2 pins are floating. This is not an issue. With that said, it would be better to ground the unused pins because they will help improve thermal performance. 

    Regards,

    Nick