Tool/software:
Hi TI Team,
We are facing issue with some boards where PGOOD is failing below 10Deg °C but are stable at 25Deg °C. Please find below observations and Circuit diagram and help in reviewing the design and suggest possible cause for this fault.
Design info:
Parameters: Vin: 12VDC, Vout: 3.3VDC, Iout(typ): ~1Amp, FSW: 650KHz, CCM.
Where used: To power rails of Intel XEON_D1527 (VCCSUS3_3, VCCCLK3_3, VCC3_3).
Observation:
1. VR_P3V3_CPLD_EN(Enable) is stable in both case 25Deg °C and 6Deg °C, i.e ~3.28VDC
2. Vout observed at C7M1 is 3.342V@ 25Deg °C and 3.280V@ 6Deg °C
3. PGOOD is observed ~3.26V@ 25Deg °C but fails ~0V@6Deg°C.
Schematic: