Other Parts Discussed in Thread: UC3875
Tool/software:
Hi Team,
Good day!
For one of our customer we are designing power converter module using PSFB topology.
Control IC we are considering as of now is UCC28950. The block diagram is as follows.

When we look at the design with the power stage designer tool, we see the Lsh inductor as below. Our question here is, does the Lsh inductor in this design have to be physically present? If an additional inductor is used, a standard type transformer will be sufficient.

Is the transformer design made LLC type and is the Lsh inductor used inside the transformer?
I want to clarify the type of transformer that should be used in this topology. Do I have to use a special transformer like in the LLC structure in this topology? Or can we use a standard transformer?
Thank you for your help!
Best Regards,
Ümit