This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: BQ34Z100-G1 P6/TS pin

Part Number: BQ34Z100-G1


Tool/software:

Hello, 

The BQ34Z100-g1 datasheet states that we need to connect the TS pin via reg25 for external NTC measurement.

The maximum input voltage range of TS1 is 1V and the ADC input resistance value is 8M ohm.

The NTC value is 10k, so this pin voltage is approximately the reg25 voltage. In short, the voltage is higher than 1V.

Is it safe? I think the 1V value is wrong.