Tool/software:
Hey,
I have built a custom pcb with bq40z80 and trying to succesfully execute the learning mode.
In section 4.2 of the slua848.pdf i have found very detailed guide of how to setup the various
registers, but when it comes to the hardware configuration, there is only this:
Discharge the battery until the voltage at the top of stack reaches the Term Voltage.
or
Charge Battery to Full
How do you do in practical term while allowing the chip firmware to observe the process properly?
I assume the guide expect everyone to use the EVAL board, so charge/discharge could be:
1. Dummy load(static) or CC/CV bench power supply to PACK+ and PACK- ?
2. As above, but between BAT+ and BMS GND ?
3. As above, but skipping the sense resistor, so BAT+ and BAT- ?
As i can read PACK, BATT and individual cells voltage, plus total and individual cells current, I assume
all those measurements are important for the learning process as well, so only option1 is viable, right ?
But section 4.2.1 calls for GAUGE_EN = 1, FET_EN=0 and RESET, so high side bidirection switch is off
during the learning process, so this will require to short PACK+ and BAT+ during the whole process ?
Thank you!