This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
We plan to use 2xUCC27614 to power primary of some high-current pulse-transformer in a full bridge configuration.
However datasheet of UCC27614 is suspiciouslysparse on details regarding self-protection.
Is there any kind of overcurrent-protectionto handle eg a short circuit at the output or to shut-down in case of overtemperature?
Hi Norman,
Our UCC27614 is a basic gate driver that only has UVLO protection. I would recommend our UCC57108 and UCC57102, which are our low-side gate drivers that have protection features like desaturation protection, overtemperature protection, and soft shutdown.
Thanks,
Rubas