Tool/software:
What is the logic of host watchdog failure recovery? How long does it take to recover?
Can I set the recover time?
HWD
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello L,
Section 5.2.16 Host Watchdog Protection in the BQ76952 Technical Reference Manual explains how it works for BQ76952 and how to set the recovery delay.
Best Regards,
Alexis
Hello L,
You won’t be able to set the time it takes for the host watchdog protection to resume. As mentioned in that section, "the device will recover (if configured for autonomous recovery) when valid communications are received". After valid communications are received, it could take up to 250 ms in NORMAL mode for the device to evaluate and clear the fault through the turn on of the FETs.
Best Regards,
Alexis