Tool/software:
Hi TI experts,
I set the speed of IIC communication between bq76942 and MCU to 400K, but when I tested the IIC waveform, I found that the delay of tSU:STA and tSU:STO did not meet the minimum 600ns requirement of the specification, as shown in the attached waveform.
The MCU pin is configured as hardware IIC, so I want to know what these two parameters are related to? How can I improve the circuit or code to meet the requirements of the specification? Do you have better suggestions?
If I do not modify any parameters, tSU:STA and tSU:STO are less than 600ns delay, will this have any impact on IIC communication? For example, IIC communication fails? Please let me know.
Thank you.