This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS562211: Simulation Error and saturation current

Part Number: TPS562211

Tool/software:

Hello TI experts,

Above is the simulation image provide from TI site, So what is a main problem is i want to change the value of ILoad but many times i changed the value , i'm not getting the expect result instead i'm getting a defaut value that which are set in simulation file

My parameter requirements is 

VIN =12V

Vout = 3.3V

ILoad = 500mA

and there is a one more question if output would be short then what will be the saturation current ?

So can you please provide simulation circuit with this requirement ?