Tool/software:
Hi,
I'm looking at using the LMR43606-Q1, and evaluating whether it should be used in PFM or FPWM mode. When the inductor current ripple is more than twice the DC load current, the device allows CCM through reverse current. However, it is my understanding that this reverse current is present at the power supply input, and could damage other components further up the power supply chain. I have 2 questions:
1. If measures are taken to protect circuitry against reverse loads (such as diodes), would this not prevent the proper CCM operation of the power supply?
2. What types of power supply are suitable as input to an SMPS operating with reverse current?
Thanks,
Leif