Tool/software:
Hi,
Seemingly the CSR can vary from 45000 A/A to 65000 A/A on a given device across the full operating temperature range. Does this mean that if I design my programmable current limit assuming a CSR of 45000 A/A, my device could experience a load current 44% higher that the designed current limit when the device temperature is at the high end of its operating range?
Thanks!