This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1663: Request for Schematic Review

Part Number: TPS1663


Tool/software:

Hello

I have selected the TPS16630 for its inrush current limiting and output off functions.

The OVP and UVLO features are not required.

I would like to request a schematic review. Are there any potential issues?

TPS1663 Review.pdf

  • Hello Jaewook,

    Please connect UVLO to IN through 500K resistance. No resistor to GND. This was UVLO will be disbaled.

    OVP you can connect to GND or make a resistor divider so OVP will always be lower than 1.2V. latter is advisable.

    Other things look good.

    You can use design calculator for dVdT cap value based on COUT.

    Thanks

    Amrit