Tool/software:
Hi,
I am planning to use the TLVM13610RDFR, which supports a programmable switching frequency from 200 kHz to 2.2 MHz via its RT pin or an external clock signal, as mentioned in the datasheet. Does this mean the RT pin can be used for either a programmable switching frequency or synchronization with an external clock signal? I would appreciate your support.
Best regards,