Hello,
Now we use TPS3106E09 in our project.
I see that the maximum transition rise and fall rate of MR is restricted to 100ns/V from the datasheet (page3).
The following shows the MR input test result of our project.
(Test 1) @U7 MR rise and fall rate measured value are 918081.21ns/V and 14031.66ns/V respectively.
(Test 2) @U8 MR rise and fall rate measured value are 877219.1 ns/V and 13683.27ns/V respectively.
From the data above, we can see that the test results are far more than the spec.
Please help to confirm the correctness of spec definition. Why does it define so quick transition rate?
Are the test results acceptable?