This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z746: HW-Protection Calibration Command

Part Number: BQ27Z746
Other Parts Discussed in Thread: BQSTUDIO

Tool/software:

How can I calibration the HW-Protection by i2c command?

I want to calibrate it in manufacturing. Thanks.

  • Hello,

    When doing the HW based protection calibration in production, the steps below should be followed  (NOTE: the steps below are ONLY for the Protector Tuning method and cannot be followed for the Protector Threshold method):

    1. Use the Protector Tuning tab in bqStudio to calibrate all of the HW based protection thresholds using an EVM or gauge that you use to collect the golden Image.
    2. Read the image from 0xF0A2 ProtectorImage2 and save this configuration somewhere (see the following bit mapping for ProtectorImage2)
    3. In production, for each gauge, you would then have to read back the value for 0xF0A2 ProtectorImage2, change only the non-reserved bits to the values you have previously saved, then write this value back into the gauge for ProtectorImage2.
    4. You would then have to save and lock the protection settings by using 0xF0A3 ProtectorImageSave.                              

    Regards, 

    Robert. 

  • Hi Robert,

    Yes, now we use this way in manufacturing.

    But we found that some protection ​​is not so accurate. So I wonder if there is a calibration command.

    Thanks & Best Regards!

  • Hello, 

    What do you mean that some are not so accurate? 

    Regards, 

    Robert. 

  • Hi Robert,

    Sorry I didn't make it clear.

    For example, the HW-Protection COV is 4.2V. But in our test, when the voltage reaches to 4.18V, it will trigger the HW-COV.

    Thanks & Best Regards!

  • Hello, 

    This is the expected behavior of the gauge as this is within 20mV accuracy. 

    Regards, 

    Robert.