This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25306: quarry

Part Number: BQ25306

Tool/software:

Greetings, Sir

We have a problem with the current used for charging.

According to the datasheet for the ICHG resistor, we need to fast charge the battery, so we added the 40K and 20K on the ICHG, but its not working, and instead we are using the 10K on the ICHG now. getting fast charge but IC is getting more heat producing.

please help us the proper current configuration for input charge of 5V 3A charger to charge the battery. and we are using the Li-po 3.7V 10000mAh battery.