This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi TI experts,
According to the datasheet of LMQ61460AFS (SNVSB70F – MAY 2019 – REVISED JUNE 2021), it will run in 'forced PWM mode' (fPWM) under both heavy and light load conditions. However when we test it under light load (<1A, PWM frequency is set to 400KHz with RT=33.2Kohm), its switching frequency will shift to below 190KHz. Is this expected behavior, or I have wrong understanding on fPWM mode?
Thanks,