This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74722-Q1: What is difference between "LM74722-Q1, LM74721-Q1, LM74720-Q1 & LM7481-Q1, LM7480-Q1 ?

Part Number: LM74722-Q1
Other Parts Discussed in Thread: LM7481-Q1, LM7480-Q1, , LM74721-Q1, LM74720-Q1, LM74502-Q1, LM74900, LM74910-Q1

Tool/software:

Hi TI Team,

I am looking for an ideal diode controller/ideal diode with the below specs.

- Input voltage support: 12V, 24V, and 48V

- RPP protection up to -65V

- Load: around 65W. 

- RPP and OVP required

I don't require automotive battery protections/features like load dump etc. My application requires RPP and OVP only. 

I am planning to go with LM747x/ LM748x family. Can you please suggest suitable part number from this family or from TI portfolio?

As well what is the major difference between "LM74722-Q1, LM74721-Q1, LM74720-Q1 & LM7481-Q1, LM7480-Q1 ?