Tool/software:
Hi Team,
Customer would like to confirm if the device will be damaged or degeneration when there is negative bias offset on Gate and Source.
For example, when the input voltage is 0V, there is open circuit detection on output port or short to battery, it may cause the MOSFET turned on due to energy transfer.
Thanks
Best,
Frank