This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM64406: TPSM64406RCH

Part Number: TPSM64406


Tool/software:

カタログを確認しましたが、パッケージが2種類あります。
I checked the catalogue,There are two types of packages.

・RCH0028A、RCH0028B

どちらが納入されますか(端子形状に違いがあります)。
Which one will be delivered?
(There are differences in the terminal shapes.)

『NON SOLDERED METALΦ0.15』と記載された丸がありますが、何ですか。
what is 『NON SOLDERED METALΦ0.15』?

また、その部位は基板のパターンに抵触するとショートするような材質ですか。
Also, is that part made of a material that would cause a short circuit if it came into contact with the circuit board pattern?