This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z561: About bqStudio

Part Number: BQ27Z561
Other Parts Discussed in Thread: BQSTUDIO

Tool/software:

About bqStudio The learning cycle procedure states to fully discharge the battery, but if the battery is fully discharged, communication may be cut off. In that case, does the learning function fail? What should I do? After charging is complete and the battery is left for more than 2 hours, the status does not become "05". Why? I have attached a record log. ⑥ Charge 2: Charge the battery at full charge voltage using constant voltage (CV) charging. Constant voltage charging is terminated at a current value between [Charge current threshold] and [Quiet current]. ⑦ Relaxation 2: Relax the battery for 2 hours until the open circuit voltage (OCV) is completely stabilized. The [LStatus] register is updated to 0x05. What is LStatus=0x14? Please tell me how to change it back to LStatus=0.

Thanks and regards