Tool/software:
Hi team,
Could you tell the recommended Rtop at the below condition to turn the device when the Vin becomes 3.0V?
Von: 3.0V
Rbottom: 10k
Regards,
Noriyuki Takahashi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi team,
Could you tell the recommended Rtop at the below condition to turn the device when the Vin becomes 3.0V?
Von: 3.0V
Rbottom: 10k
Regards,
Noriyuki Takahashi
Hello,
Thank you for your question.
The FB_PG pin is used to adjust the current limit for the TPS7A96 device.
Please see page 30 in the datasheet for additional information:
What would the customer like to set the current limit of the device to?
How is the customer intending on using the FB_PG pin?
Please let me know when you have a moment.
Thank you,
Hannah
Hannah,
Their questions is about equation 1 and 2 in the datasheet and undersntad how to decide the Rtop at the below condition to turn the device when the Vin becomes 3.0V. Does this make sense? Could you give the recommended value with the caluculation process?
Von: 3.0V
Rbottom: 10k
Regards,
Noriyuki Takahashi
Hello Noriyuki,
Thank you for the further explanation. This makes sense to me now. Assuming a VEN,HI voltage of 1.22V, stated in the datasheet, then using equation 1:
Rtop < (10k) x ((3/1.22)-1), Rtop < 14.6k, which means they should choose an Rtop value that is less than or equal to 14.6k ohm.
Hope this helps.
Best regards,
Hannah