Other Parts Discussed in Thread: UCC28730
Tool/software:
Hi expert,
UCC28730 has this curve for EA output to current output.
Between 1.3-2.2V, IPP control a fixed on-time and FM increase the switch frequency to increase the output current.
Between 2.2V-3.55V, frequency is fixed to 28kHz and IPP goes up to increase the on-time and increase the output current.
In this two mode, the on-time and switching period is fixed by control method, how does valley switch works? I think valley switch will directly turn on the mosfet and influence the control loop.

For the final 3.55-4.85V, 28730 is just work like 1.3-2.2V, so during the whole range, do we need to design it all in DCM mode? (even in the CC mode, 4.85-5V?)
Thanks!