This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28951: Is a PSFB the best option for a Lithium battery charger?

Part Number: UCC28951

Tool/software:

Hello, I'm designing a battery charger and have selected a PSFB topology based on the IC UCC28951. However, during the design, I saw that LLC could have better efficiency. 
It seems that LLC has better efficiency, but it works better on a fixed output voltage. In my case the output voltage will have to change from 40V to 60V so I'm not sure if it will have a high impact on the efficiency. 
On the other hand, the PSFB has good efficiency but it's more expensive because it needs 4 HV fets and their drivers. 
Do you think that the LLC will have a big negative impact on the efficiency of this output voltage range?

  • Hi Bangalii,

    What is the power level you are looking to support? In general you are correct in that the PSFB is traditionally better than an LLC for supporting a wider output voltage range. That being said, our new LLC the UCC25660 with IPPC (Input Power Proportional Control) makes it well suited to support a wider output voltage range while avoiding entering burst mode with low VBATT during the CC charging phase. 

    In the past when an LLC controller was used for a battery charging, to avoid entering burst mode with low VBATT, it would be used in an LCC configuration. While the LCC can support a wider output voltage range, it will have a lower efficiency compared to an equivalent power level LLC. The good news is that our new controller can support the wider output range as an LLC!

    We do have a reference design PMP23464 showing our new controllers capability. 

    I hope this answers your question.