Other Parts Discussed in Thread: UC2875,
Tool/software:
hi,
we are replacing UC2875 with UCC28951 as unique option.
For our product, we absolutely need a controller that can operate at a switching frequency of 20 kHz, while the UCC28951 is recommended from 50KHz on.
my question is then: can the UCC28951 operate at 20KHz (RT >>100KOhm, accordingly to eq. 10 & 11)?
If no go, which ZVS with 4 outputs would you suggest?
thx a lot
Vincenzo