Tool/software:
Hi,
In one of our design we have configured TPS25730DREFR as mention below
ADCIN1: To set the Minimum Voltage = 9V
Rup = 100K
Rdown = 4.7K
ADCIN2: To set the Maximum Voltage = 15V
Rup = 100K
Rdown = 100K
ADCIN3: To set the Operating Current = 2.5A
Rup = 100K
Rdown = 12K
ADCIN4: To set the Maximum Operating Current = 3A
Rup = 100K
Rdown = 100K
Please clarify
1. Will the power path be enabled if we use a 5V/3A adapter that doesn't support PD?
2. By default will the internal power path MOSFETs are enable or do you have any Conditions?
Thanks & Regards,
Gayathri Palla.