Tool/software:
Hi team,
can the ILIM pin NC in the real application? or it must to be connected to GND when not use? and I found When the charge is NC to system and battery, the input current, leakage current is about 20mA when NC ILIM pin, which seems lead to it can't activate the battery when over discharge. could you give some suggestions about that?
BR
Jingguo