This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR66430: Customize LMR66430MC5RXBRQ1

Part Number: LMR66430

Tool/software:

Hello TI engineers
I have a question about LMR66430MC5RXBRQ1.

I am using WEBENCH POWER DESIGNER to use this IC with external synchronization.
I have entered the input and output conditions and pressed the “VIEW DESIGN LMR66430MC5RXBRQ1” button.
When I press the “VIEW DESIGN LMR66430MC5RXBRQ1” button, I get a schematic, but the frequency is set to 2.2MHz.

I want to use an external sync clock at 450 kHz and I want to simulate at 450 kHz.
Is there a way to do this?

  • Hello

    Let me find the Application engineer for this product and we will get back to you as soon as possible.

    Thanks

  • Hi, 

    That design is not supported with the LMR66430MC5RXBRQ1 model at this time, but adjustable switching frequency is available with the LMR66430R5RXBR model. These two models should perform similarly. The only difference is that the LMR66430R5RXBR will have PFM mode giving better light load efficiency. You can change your switching frequency when opening a design using the tab to the left. For your convenience I have also started a design for you: webench.ti.com/.../SDP.cgi

    Thank you,

    Joshua Austria